Thomson currently has two account systems - one for the website and CAD model downloads, and one for e-commerce. We understand that two logins is an inconvenience and are working to consolidate our systems into one login process. Until we’re able to consolidate the two logins, please follow these guidelines:
Thomson ball screw assemblies consist of a ball screw, a ball nut with recirculating ball bearings and end supports for mounting. The interface between the screw and the nut is made by ball bearings that roll in matching forms in the ball screw and ball nut. The load on the ball screw is distributed over a large number of ball bearings so that each ball is subjected to a relatively low load. Because of the rolling element design, ball screw assemblies have a very low coefficient of friction, which equates to highly efficient mechanics.
Ball screw assemblies provide an excellent method for translating rotational motion to linear motion for many applications, including those where high loads and close tolerances are required. To apply the correct type of ball screw and nut assembly in a particular application, the design engineer must consider the advantages and capabilities of each. Selecting the right technology can reduce design complexity, improve performance and reduce the overall cost of the assembly.
This image compares the three types of ball return systems (from left to right): internal, button and external.
Ball screws are mounted in either supported or fixed configurations. A supported end holds the ball screw at one focal point and does not resist bending moments. A supported end is generally easier to align and install than a fixed one, so installation costs are typically lower. A fixed end resists bending moment loads because it is typically based on two bearings spaced sufficiently so the ball screw remains perpendicular to the planes of the rotary bearings. The fixed offers greater column strength and higher critical speed. The image below illustrates four fixity options.
The assembly can be fixed at both ends, fixed at only one end and supported on the other, supported at both ends, or fixed at one end and free at the other.
Ball screw assemblies are not all alike. Whether it be metric ball screws, inch ball screws or miniature ball screws, key differences affect their performance and extend their lives. These include:
Chaque nouvelle application exige une analyse minutieuse des performances, du cycle de vie et du coût des produits. En particulier de ceux qui sont amenés à supporter des charges élevées. Découvrez pourquoi vous devriez envisager d'utiliser une vis à billes à charge élevée au lieu d'une vis à billes standard dans votre prochaine application de mouvement linéaire.
Présentateur : Markus Brändle, Spécialiste gamme de produits – Vis, vérins à vis et LB&G Thomson Neff Industries, Allemagne
Comment recharger les roulements dans un écrou à billes à retour par bouton. Les écrous à billes métriques sont souvent à retour par bouton. Mais cette technique peut également être utilisée sur les écrous à billes à retour par tube.
Parmi les milliers de choix possibles, comment dimensionner et trouver rapidement et sans risque de se tromper la solution de vis à billes optimale pour votre application de mouvement linéaire ?
Comment installer un écrou à billes sur la vis d'un arbre lisse.
Étant donné que les vis à billes sont disponibles en dimensions impériales et métriques, les concepteurs commencent parfois le processus de spécification en sélectionnant une gamme de produits sur la base de l'unité de mesure. Cette approche présente le risque d'exclure prématurément le produit idéal pour l'application et d'entraîner des pertes considérables en temps, main-d'œuvre et coûts. Cet article explique comment en centrant les questions de dimensionnement et de choix sur les performances plutôt que sur le nom des produits, il est possible de créer des solutions de mouvement linéaire plus efficaces.
En savoir plusLes vis à rouleaux sont souvent présentées comme étant la seule technologie à même de supporter des charges élevées dans les applications soumises à une contrainte de taille. Toutefois, les progrès réalisés dans la technologie des vis à billes les rendent désormais également compatibles avec des applications impliquant des charges élevées. Cet aspect est important, car une vis à billes à charge élevée coûte habituellement deux fois moins cher qu'une vis à rouleaux comparable à performances équivalentes.
En savoir plusUtilisés dans les applications de production à grande échelle comportant des opérations de levage continues mais toujours susceptibles de nécessiter une intervention humaine, les robots collaboratifs (cobots) sont de plus en plus répandus. Un fabricant français de cobots a élaboré une solution faisant appel à des vis à billes et à des vérins à câble au lieu d'engrenages et qui fait figure de référence en termes d'efficacité et de sécurité des cobots.
En savoir plusVis de précision | 7869 KB | |
Vis de précision | 7890 KB | |
Vis de précision | 6740 KB |
Thomson High-Load Ball Scews Provide Maximum Load Capacity and Longer Life in a Compact Envelope | 2019-02-04 |
To provide better service to you on our websites, we and our service providers use cookies to collect your personal data when you browse. For information about our use of cookies and how to decline them or turn them off please read our cookie policy [available here].