Thomson currently has two account systems - one for the website and CAD model downloads, and one for e-commerce. We understand that two logins is an inconvenience and are working to consolidate our systems into one login process. Until we’re able to consolidate the two logins, please follow these guidelines:
Thomson ball screw assemblies consist of a ball screw, a ball nut with recirculating ball bearings and end supports for mounting. The interface between the screw and the nut is made by ball bearings that roll in matching forms in the ball screw and ball nut. The load on the ball screw is distributed over a large number of ball bearings so that each ball is subjected to a relatively low load. Because of the rolling element design, ball screw assemblies have a very low coefficient of friction, which equates to highly efficient mechanics.
Ball screw assemblies provide an excellent method for translating rotational motion to linear motion for many applications, including those where high loads and close tolerances are required. To apply the correct type of ball screw and nut assembly in a particular application, the design engineer must consider the advantages and capabilities of each. Selecting the right technology can reduce design complexity, improve performance and reduce the overall cost of the assembly.
This image compares the three types of ball return systems (from left to right): internal, button and external.
Ball screws are mounted in either supported or fixed configurations. A supported end holds the ball screw at one focal point and does not resist bending moments. A supported end is generally easier to align and install than a fixed one, so installation costs are typically lower. A fixed end resists bending moment loads because it is typically based on two bearings spaced sufficiently so the ball screw remains perpendicular to the planes of the rotary bearings. The fixed offers greater column strength and higher critical speed. The image below illustrates four fixity options.
The assembly can be fixed at both ends, fixed at only one end and supported on the other, supported at both ends, or fixed at one end and free at the other.
Ball screw assemblies are not all alike. Whether it be metric ball screws, inch ball screws or miniature ball screws, key differences affect their performance and extend their lives. These include:
Toda aplicación nueva requiere un análisis detallado del rendimiento, la vida y el costo del producto. Especialmente, aquellas que implican grandes cargas. Conozca por qué debería considerar un husillo de bolas de alta carga por sobre los husillos de bolas estándar para su próxima aplicación de movimiento lineal.
Presentador: Markus Brändle, especialista en línea de productos– husillos, elevadores mecánicos y LB&G Thomson Neff Industries, Alemania
¿Cómo recargar los rodamientos en una tuerca de bolas con retorno de botón? A menudo, las tuercas de bolas métricas son tuercas de bolas con retorno de botón. Pero esta técnica también se puede usar en tuercas de bolas con retorno de tubo.
Hay miles de opciones posibles. ¿Cómo medir con rapidez y seguridad el tamaño y elegir la solución de husillo de bolas ideal para su aplicación de movimiento lineal?
¿Cómo instalar una tuerca de bolas en un husillo de un árbol?
Dado de los husillos de bolas están disponibles en ambas dimensiones, pulgadas y sistema métrico, a veces, los diseñadores comienzan el proceso de especificación por seleccionar una familia de productos con base en la unidad de medida. Esta decisión puede, de forma prematura, excluir al producto ideal para la aplicación y conducir a importantes pérdidas de tiempo, trabajo y dinero. Este artículo explica cómo las preguntas en torno a la medición y la selección centradas en el rendimiento, y no en el nombre del producto, pueden conducir a diseños de movimiento lineal más eficientes.
Más informaciónLos husillos de rodillos se han promovido como la única opción tecnológica para manejar grandes cargas cuando el tamaño es una limitación.Pero, en la actualidad, los avances en la tecnología de los husillos de bolas han permitido la capacidad de tolerar aplicaciones de cargas altas. Esto es importante porque los husillos de bolas de carga alta cuestan, normalmente, menos de la mitad de lo que cuesta un husillo de rodillos en puntos de rendimiento equivalente.
Más informaciónLos robots colaborativos (cobots) están ganando popularidad. Se utilizan en aplicaciones de producción a gran escala que involucran continuas operación de elevación, pero que siguen requiriendo la participación humana. Un fabricante francés de cobots ha desarrollado una solución que utiliza husillos de bolas y actuadores con cable en lugar de engranajes; con esta solución estableció un nuevo punto de referencia para la eficiencia y la seguridad de los cobots.
Más informaciónThomson High-Load Ball Scews Provide Maximum Load Capacity and Longer Life in a Compact Envelope | 2019-02-04 |
To provide better service to you on our websites, we and our service providers use cookies to collect your personal data when you browse. For information about our use of cookies and how to decline them or turn them off please read our cookie policy [available here].