KRISTIANSTAD, SWEDEN - Thomson Industries, Inc., a leading manufacturer of linear motion control solutions, has announced a new family of compact systems that makes it easier for motion designers to implement complex applications in small spaces. Designers needing thrust and bearing support in a single, compact unit now have flexibility to build such applications with versatile, time-tested components from Thomson.
"As demand for smaller-scale applications grows, so does the challenge of packing high functionality into a smaller footprint. Our new family of compact linear motion systems equips designers to meet those challenges by assembling world-renowned Thomson linear motion components, with the added option of real-time collaboration with a Thomson engineer,” said Hans Dahlen, Product Line Manager – Linear Motion Systems for Thomson.
In building a compact linear system from Thomson, a designer can configure a unit or combination of units from a wide variety of components based on their specific application details. Components include, but are not limited to:
- Integrated stepper motors
- Lead screws
- Profile rail linear guides
- 60 Case® LinearRace® shafting
- Linear Ball Bushing® bearings
- End blocks
Many features can be customized, including screw diameters and leads, mounting holes and mounting configurations.
Machine designers who need thrust and bearing support in a single, compact unit can now build a personalized system from Thomson premier linear modules in real time, under the guidance of an expert engineer running 3D modelling tools. (Image courtesy of Thomson Industries, Inc.)
To enable engineers to take maximum advantage of such flexibility, Thomson offers an innovative new 3D modelling tool that optimizes their solution by revealing design trade-offs in real time. The tool, in collaboration with a Thomson engineer, guides the designer in tailoring motor size, stroke length, and other variables to function most effectively within given load and space parameters.
The resulting designs go directly to the Thomson product CAD system, where the information is used to produce the prototype sent for testing. Because of such close user involvement during the design process, the number of design iterations is reduced, which, in turn, decreases the likelihood of mistakes being made.
Applications
Thomson compact linear systems are appropriate for applications requiring high-accuracy linear axes in confined spaces, such as 3D printers, microscope stage managers, medical pipetting systems and semiconductor manufacturing. They are available with NEMA motor sizes between 14 and 23; stroke lengths of up to 1000 mm; and load capacities up to 9300 Newtons.
For more information on Thomson compact linear system, please click here: https://www.thomsonlinear.com/en/products/compact-linear-systems
About Thomson Industries, Inc.
With more than 75 years of achievement in motion control innovation and quality, Thomson is the industry’s premier producer of Linear Actuators, Linear Ball Bushing® Bearings and Profile Rail Bearings, 60 Case® Shafting, Ground and Rolled Ball Screws, Linear Systems, and related accessories. Thomson invented the Linear Ball Bushing Bearing in 1945 and has set the standard ever since with an unsurpassed set of linear motion control solutions serving global aerospace and defence, medical and health, factory automation, food processing, and mobile off-highway markets. Thomson, a brand of U.S.-based Altra Industrial Motion, has facilities in North America, Europe and Asia with more than 2000 distributor locations around the world.
For more information Thomson Industries, Inc., 1500 Mittel Boulevard, Wood Dale, IL 60191-1073; 1-540-633-3549; 1-540-633-0294 (fax); Thomson@thomsonlinear.com; www.thomsonlinear.com.