Skip to content Skip to navigation

02/12/2019 | New Thomson video spotlights customer’s use of electric linear actuators’ synchronisation option

Kristianstad, Sweden – Thomson Industries, Inc., a leading manufacturer of linear motion control solutions, has released a video showing how the synchronisation feature available with its Electrak® HD electromechanical linear actuators helped Spika Design and Manufacturing address a growing customer demand. Spika is a Montana-based provider of commercial and custom industrial work platforms suitable for a wide variety of assembly and maintenance operations.

Spika Design and Manufacturing, one of the leaders in the industry for elevated access equipment, relies on electromechanical linear actuators with synchronisation option from Thomson.

Prior to adopting electromechanical actuators, height variability for Spika’s work platforms relied upon manual screw jacks and hydraulics, which carried many drawbacks. Load distribution and uneven platforms still posed challenges for customers, even with standard self-synchronising electric actuators. As a result, Spika engineers began to search for alternative solutions to optimise their platform designs.

“In the past, we have used hydraulics, and we found that they were messy for the end user, and we had a hard time keeping the platform level from one side to the other,” said Kyle Whitecraft, Director of Quality Assurance at Spika. “With more unique customer needs, where we need up to three or five metres of adjustability, we realised we needed to source other actuators with more strength, synchronisation options and longer strokes to continue meeting our customers’ expectations.”

“When Thomson introduced their line of Electrak HD actuators, it was very well custom made for our requirements,” said Tom Spika, the company’s founder and CEO, referring to the product’s optimised speed, power and control for dynamic loading with the right stroke lengths. “Thomson also offered simplistic installation, everything was integrated within the actuators and took very little time to assemble into our system.”

“The Electrak HD provided greater static strength, which was important for Spika,” said Chad Carlberg, Product Line Manager - Linear Actuators with Thomson. “Anytime they faced a cantilever or an uneven load, they needed synchronisation. The Electrak HD also moved faster than previous actuators. Plus, when Spika faced hard challenges with delivery and long lead times for their customers, we were able to deliver in 2-3 weeks.”

As Spika’s platforms became more proficient, they received additional requests from customers and were able to get rid of the counter weights for the cantilever parts; as well as resolve the on-board counter weighting to address the uneven loading conditions. With Thomson’s synchronisation feature, the speed of actuation remains constant even in the presence of uneven loads on the actuator. This was particularly important in applications where different actuators in sync on the same platform experience different types of loads such as small or large, compression or tension, while still delivering stable movement.

“Synchronisation has allowed us to ensure accuracy,” added Spika. “With the Electrak HD series, we can also connect more than one deck together, link actuators and elevate all platforms at one time to ensure they are all consistently elevating.”

Spika’s customers require a safe access platform capable of a variety of heights that allows them to work ergonomically. Occupational Safety and Health Administration (OSHA) regulations had required Spika to load test all of their platforms to a 4x safety factor. One of the immediate benefits that Thomson’s actuator provided was static load ratings, holding loads up to 18 kN / 4050 lbf. “With our Electrak HD electromechanical actuators, we have been able to help Spika provide customers with greater variation of work platforms with stronger static control and faster delivery,” said Carlberg.

In the future, Spika hopes to expand use of Electrak HD actuators with servo motor control and PLCs. “As we go forward, we are going to be designing new and unique products to address the application needs of our customers,” said Tom Spika. “Without a doubt, Thomson is going to be a part of that process of development.”

To view the video, please visit: https://youtu.be/QpKOz5-qR54

For more information about Thomson’s Electrak HD Linear actuators, please visit: https://www.thomsonlinear.com/en/products/linear-actuators/electrak-hd-products.

About Thomson Industries, Inc.
With more than 70 years of motion control innovation and quality, Thomson Industries is the industry’s premier producer of Linear Ball Bushing® Bearings and Profile Rail Bearings, 60 Case® Linear Shafting, Ball Screws, Lead Screws, Screw Jacks, Linear Actuators, Linear Systems, and related accessories. Thomson invented the Linear Ball Bushing Bearing in 1945 and has set the standard ever since with an unsurpassed set of linear motion control solutions serving global commercial and aerospace and defence markets. Thomson Industries, Inc. has facilities in North America, Europe and Asia with more than 2000 distributor locations around the world.

Thomson Industries, Inc., 1500 Mittel Boulevard, Wood Dale, IL 60191-1073; 1-540-633-3549; 1-540-633-0294 (fax); Thomson@thomsonlinear.com; www.thomsonlinear.com.

Spika provides ergonomic work platforms, supporting a wide variety of assembly and maintenance operations for automotive, aerospace and military aviation manufacturers.

Thomson Electrak HD electromechanical linear actuators deliver smooth synchronisation for Spika work platforms.

In instances where there are heavily cantilevered and uneven loads, such as this platform for accessing the nose of an aircraft, actuator synchronisation is key.

back to top