Thomson currently has two account systems - one for the website and CAD model downloads, and one for e-commerce. We understand that two logins is an inconvenience and are working to consolidate our systems into one login process. Until we’re able to consolidate the two logins, please follow these guidelines:
Thomson ball screw assemblies consist of a ball screw, a ball nut with recirculating ball bearings and end supports for mounting. The interface between the screw and the nut is made by ball bearings that roll in matching forms in the ball screw and ball nut. The load on the ball screw is distributed over a large number of ball bearings so that each ball is subjected to a relatively low load. Because of the rolling element design, ball screw assemblies have a very low coefficient of friction, which equates to highly efficient mechanics.
Ball screw assemblies provide an excellent method for translating rotational motion to linear motion for many applications, including those where high loads and close tolerances are required. To apply the correct type of ball screw and nut assembly in a particular application, the design engineer must consider the advantages and capabilities of each. Selecting the right technology can reduce design complexity, improve performance and reduce the overall cost of the assembly.
This image compares the three types of ball return systems (from left to right): internal, button and external.
Ball screws are mounted in either supported or fixed configurations. A supported end holds the ball screw at one focal point and does not resist bending moments. A supported end is generally easier to align and install than a fixed one, so installation costs are typically lower. A fixed end resists bending moment loads because it is typically based on two bearings spaced sufficiently so the ball screw remains perpendicular to the planes of the rotary bearings. The fixed offers greater column strength and higher critical speed. The image below illustrates four fixity options.
The assembly can be fixed at both ends, fixed at only one end and supported on the other, supported at both ends, or fixed at one end and free at the other.
Ball screw assemblies are not all alike. Whether it be metric ball screws, inch ball screws or miniature ball screws, key differences affect their performance and extend their lives. These include:
Qualquer aplicação nova requer uma análise cuidadosa do desempenho, da vida e do custo do produto. Especialmente aqueles que lidam com cargas maiores. Descubra por que você deveria estar pensando em um parafuso de esfera de alta carga em vez de parafusos de esfera padrão para a sua próxima aplicação de movimento linear.
Apresentador: Markus Brändle, especialista em linha de produção – Screws, Screw Jacks e LB&G Thomson Neff Industries, Alemanha
Como recarregar rolamentos de esferas em uma porca esférica. As porcas esféricas métricas costumam ser porcas esféricas de retorno de botão. Mas essa técnica também pode ser usada em porcas esféricas de retorno de tubo.
De todas as milhares de escolhas possíveis, como você poderia avaliar e selecionar o parafuso de esfera ideal para a sua aplicação de movimento linear?
Como instalar uma porca esférica em um parafuso com um mandril.
Como todas as porcas esféricas estão disponíveis tanto nas dimensões em polegadas quanto métricas, às vezes os designers começam o processo de especificação selecionando uma família de produto com base na unidade de medida. Essa decisão pode excluir prematuramente o produto ideal para a aplicação e levar a perdas significativas em termos de tempo, trabalho e custos. Este artigo explica como as perguntas sobre dimensionamento e seleção centradas no desempenho – em vez de nomes de produtos – podem levar a designs de movimento linear mais eficientes.
Saiba maisParafusos de rolo foram promovidos como a única tecnologia a ser escolhida para lidar com grandes cargas e com limitações de tamanho. Mas, na verdade, avanços na tecnologia de parafuso de esfera agora permitem a capacidade de suportar também as aplicações de alta carga. Isso é importante porque um parafuso de esfera de alta carga costuma custar menos do que a metade de um parafuso de rolo com pontos de desempenho equivalentes.
Saiba maisUsados em aplicações de produção em larga escala envolvendo operações de elevação, mas que ainda necessitam de um toque humano, os robôs colaboradores (cobots) estão ganhando popularidade. Um francês criador de cobots desenvolveu uma solução que usa parafusos de esfera e atuadores de cabo em vez de engrenagens, criando uma nova referência de eficiência e segurança de cobots.
Saiba maisThomson High-Load Ball Scews Provide Maximum Load Capacity and Longer Life in a Compact Envelope | 2019-02-04 |
CONJUNTOS DE PARAFUSOS ESFÉRICOS | |||
Conjuntos de parafusos esféricos – Polegada | ![]() |
— | — |
Conjuntos de parafusos esféricos – Métricos (América do Norte) | ![]() |
— | — |
Conjuntos de parafusos esféricos – Métricos (Europa) | ![]() |
— | — |
PORCAS ESFÉRICAS | |||
Porcas esféricas flangeadas – Polegada | ![]() |
— | — |
Porcas esféricas flangeadas – Métricas | ![]() |
— | — |
Porcas esféricas roscadas – Polegada | ![]() |
— | — |
Porcas esféricas roscadas – Métricas | ![]() |
— | — |
Porcas esféricas cilíndricas – Métricas | ![]() |
— | — |
SUPORTES NA EXTREMIDADE | |||
Suportes na extremidade de parafusos esféricos – Polegada | ![]() |
— | — |
Suportes na extremidade de parafusos esféricos – Métricos | ![]() |
— | — |
PARAFUSOS | |||
Parafusos esféricos laminados Precision – Polegada | ![]() |
— | — |
Parafusos esféricos laminados Precision – Métricos | ![]() |
— | — |
ACESSÓRIOS | |||
Flanges de parafuso esférico | ![]() |
— | — |
Limpadores de parafuso esférico | ![]() |
— | — |
To provide better service to you on our websites, we and our service providers use cookies to collect your personal data when you browse. For information about our use of cookies and how to decline them or turn them off please read our cookie policy [available here].