Thomson currently has two account systems - one for the website and CAD model downloads, and one for e-commerce. We understand that two logins is an inconvenience and are working to consolidate our systems into one login process. Until we’re able to consolidate the two logins, please follow these guidelines:
The accuracy class of a profile rail bearing is defined by three tolerances:
Running Parallelism
Assembly Accuracy
Pair Variation
These are measured from the rail base to the center of the carriage top (H), and from the rail reference edge to the the carriage reference edge (A). See the figure below for "H" and "A" dimension locations.
Running Parallelism
describes the tolerance on H and A as a function of axial travel,
measured from one carriage down the length of the rail. This is
analogous to straightness of travel. As such, parallelism describes
attributes of the rail only.
Assembly accuracy describes the tolerance on H and A as a function of a carriage – rail assembly, measured from the nominal dimensions.
Pair Variation
Pair variation describes tolerance on H and A as a function of carriages at the same position on a common rail. Pair variation describes carriage precision only.
System Accuracy
The accuracy class selected will partially determine the accuracy of the system. Other factors such as mounting surface flatness and straightness also significantly affect system accuracy.
To provide better service to you on our websites, we and our service providers use cookies to collect your personal data when you browse. For information about our use of cookies and how to decline them or turn them off please read our cookie policy [available here].