A preloaded bearing loaded beyond the preload value has the same characteristics as a clearance bearing. In the example above, if the applied load is greater than 1.7kN then the preload has no benefit.The carriage has dynamic load capacity of 21.1kN,The Preloaded is specified as 0.08 C or 0.08 x 21.1kN = 1.7kN
Preload = 1.7kN