Skip to content Skip to navigation

Design and Theory

The following are some definitions of common terms used with ball screws.

Static load Rating

Static Load Rating is the maximum load capacity the ball screw can hold while NOT turning.  Applying a load above the static rating can cause brinelling of the ball track or splitting the ball bearings in half.

NEVER exceed the Static Load Rating


Example of Brinelling

Dynamic load rating

Dynamic load rating is the load that an assembly can maintain for:
  • 1 million inches of travel - imperial
  • 1 million revolutions - Metric
The failure mode for exceeding the dynamic load rating or travel distance at that load is Spalling of the ball groove.  Exceeding the dynamic load rating is not recommended.

Example of spalling

Ball Circle Diameter

Ball Circle diameter or BCD is the distance between the centerlines of two opposing balls in contact with the screw.  The dimension is shown in the image below.

Ball Circle Diameter

Thread direction

The thread direction refers to the direction of the thread helix around the shaft.  As with regular bolts and nuts right hand is used as standard and left hand is only used when there is a specific requirement a left hand thread.  In ball screws there is rarely a need for a Left hand threaded screw.  Often there are only a few sizes offered with Left hand thread.

Right hand and Left hand thread screws

If there is a need for an assembly where both ball nuts come together and move apart as the shaft is turned in one direction, a right hand and left hand screw can be useful.  A right hand and left hand screw can be created by forming the right hand threads and left hand threads into one shaft or by coupling 2 shafts together.  Either method may have an area in the center where there may be no thread or imperfect threads.

Right hand and left hand thread assembly

back to top