Thomson currently has two account systems - one for the website and CAD model downloads, and one for e-commerce. We understand that two logins is an inconvenience and are working to consolidate our systems into one login process. Until we’re able to consolidate the two logins, please follow these guidelines:
In RoundRail linear bearings, the load capacity changes when the bearing is rotated around the shaft relative to the load. The published Dynamic load capacity of a Thomson Ball Bushing Bearing is only valid when used in the optimal orientation. Loading at an orientation other than the optimal orientation will require de-rating the load capacity.
If we graph the load capacity of the Ball Bushing® bearing vs the orientation to the ball tracks, we end up with a graph like below.
Load capacity of the Ball Bushing® bearing vs the ball tracks
Load capacity of the Ball Bushing® bearing vs the ball tracks
The image on the
left shows the load pressing between the two bearing plates. In this
case, the load will be shared by two bearing plates. This orientation is
the optimal orientation and where the bearing can carry its maximum load.
The image on the right, the bearing has been rotated and the load
is applied directly over one of bearing plates. In this situation, the
load is riding mostly on the one bearing plate. This orientation is
where the bearing is at its lowest capacity.
To calculate the load
capacity for a particular orientation, read the correction factor off
the graph then multiply by the published rated load capacity. Note: the load correction factor graph varies based on the product design and number of ball tracks. See the product
specifications to see the load correction factor graph for a specific product.
To provide better service to you on our websites, we and our service providers use cookies to collect your personal data when you browse. For information about our use of cookies and how to decline them or turn them off please read our cookie policy [available here].