![Are linear ball bushing bearing pillow blocks sealed?](/ds_images/images_relaunch/Are_linear_ball_bushing_bearing_pillow_blocks_sealed-585x400.jpg)
The Super Smart, Super, Precision, and XR ball bushing pillow blocks include a seal in each end of the block. The seal is an external seal and is press fit into each end of the pillow block. If pillow blocks are not used, select ball bushing bearings can be supplied with optional integral seals.