Zum Inhalt springen Zur Navigation springen

Deep-Dive Into High-Power Electric Linear Actuator Design Considerations (EU) | 40 min



Are your linear motion applications reaching their potential?

Electric linear actuators have come a long way since their origin as basic, slow, medium load pushing-and-pulling devices more than a half century ago. Protection against the elements has greatly improved, integrated controls have added intelligence to their functionality, and life, reliability and performance have all steadily improved. The next generation of electric linear actuators has changed the game. Learn how electric actuators are now taking over linear applications that were once dominated by hydraulic systems.

Watch this 40-minute webinar recording and learn about:

  • The key design considerations when specifying the optimal actuator solution to meet your application demands.
  • The key features of new electric actuators that make them ideal for conversion from hydraulic systems.
  • The groundbreaking performance and control capabilities that make select electric linear actuators unique.
  • The markets and applications in which high-power electric actuators are now excelling.

Presenter: Robert Johansson, Conversion Specialist, Thomson Industries

Zum Seitenanfang