Thomson currently has two account systems - one for the website and CAD model downloads, and one for e-commerce. We understand that two logins is an inconvenience and are working to consolidate our systems into one login process. Until we’re able to consolidate the two logins, please follow these guidelines:
Thomson ball screw assemblies consist of a ball screw, a ball nut with recirculating ball bearings and end supports for mounting. The interface between the screw and the nut is made by ball bearings that roll in matching forms in the ball screw and ball nut. The load on the ball screw is distributed over a large number of ball bearings so that each ball is subjected to a relatively low load. Because of the rolling element design, ball screw assemblies have a very low coefficient of friction, which equates to highly efficient mechanics.
Ball screw assemblies provide an excellent method for translating rotational motion to linear motion for many applications, including those where high loads and close tolerances are required. To apply the correct type of ball screw and nut assembly in a particular application, the design engineer must consider the advantages and capabilities of each. Selecting the right technology can reduce design complexity, improve performance and reduce the overall cost of the assembly.
This image compares the three types of ball return systems (from left to right): internal, button and external.
Ball screws are mounted in either supported or fixed configurations. A supported end holds the ball screw at one focal point and does not resist bending moments. A supported end is generally easier to align and install than a fixed one, so installation costs are typically lower. A fixed end resists bending moment loads because it is typically based on two bearings spaced sufficiently so the ball screw remains perpendicular to the planes of the rotary bearings. The fixed offers greater column strength and higher critical speed. The image below illustrates four fixity options.
The assembly can be fixed at both ends, fixed at only one end and supported on the other, supported at both ends, or fixed at one end and free at the other.
Ball screw assemblies are not all alike. Whether it be metric ball screws, inch ball screws or miniature ball screws, key differences affect their performance and extend their lives. These include:
Dieses Video behandelt den Aufbau und die Installation von Kugelgewindetrieben. Es erlätert die Funktion von Kugelgewindetrieben im Anwendungsdesign sowie die Komponenten eines Kugelgewindetriebes und einer Kugelgewindemutter. Außerdem wird die Montage einer Kugelgewindemutter auf eine Spindel dargestellt und das Einsetzen von Kugellagern für den Fall, dass einige Lager während der Montage herausfallen.
Jede einzelne Anwendung erfordert eine sorgfältige Analyse von Leistung, Lebensdauer und Kosten. Das gilt insbesondere bei hohen Lasten. Erfahren Sie, warum Sie bei Ihrer nächsten Nutzung eines Linearsystems einen Schwerlast- einem Standard-Kugelgewindetrieb vorziehen sollten.
Referent: Markus Brändle, Produktlinien-Verantwortlicher – Kugelgewindetriebe, Spindelhubgetriebe sowie Linearlager & -führungen bei Thomson Neff Industries, Deutschland
Wiederbefüllen einer Kugelgewindemutter mit Lagerkugeln. Metrische Kugelgewindemuttern sind häufig mit einer Einzelumlenkung ausgestattet. Die gezeigte Methode eignet sich aber auch für Muttern mit Kanalumlenkung.
Wie wählen Sie aus all den Tausenden von Möglichkeiten schnell und zuverlässig für Ihre Linearanwendung den optimalen Kugelgewindetrieb in der passenden Größe?
So gelangt die Kugelgewindemutter sicher von der Transporthülse auf die Spindel.
Da Kugelgewindetriebe sowohl in Zoll als auch in metrischen Maßen erhältlich sind, beginnen Konstrukteure zuweilen ihre Spezifikation mit der Auswahl einer Produktreihe nach diesem Unterscheidungsmerkmal. Diese Entscheidung kann jedoch das perfekte Produkt für die jeweilige Anwendung von vornherein ausschließen und zu deutlichen Nachteilen bezüglich Zeit-, Arbeits- und Kostenaufwand führen. Dieser Artikel erläutert, wie Auslegungs- und Auswahlfragen, die auf die Leistung abzielen – anstatt auf Produktnamen – effizientere Linearlösungen ergeben.
Mehr erfahrenRollengewindetriebe galten seit langem als einzige Technologie zur Bewegung großer Lasten, wenn die Baugröße begrenzt ist. Tatsächlich haben Fortschritte in der Technologie von Kugelgewindetrieben die Möglichkeit eröffnet, auch für Anwendungen mit hohen Lasten eingesetzt zu werden. Das ist besonders wichtig, da ein Hochlast-Kugelgewindetrieb in der Regel nur halb so teuer ist wie ein Rollengewindetrieb mit vergleichbaren Leistungswerten.
Mehr erfahrenIn der Massenproduktion, wo repetitive Hubbewegungen ausgeführt werden, aber dennoch manuelle Eingriffe erforderlich sind, erlangen sogenannte „kollaborative Roboter“ (Cobots) immer mehr an Beliebtheit. Ein französischer Cobot-Hersteller hat nun eine Lösung entwickelt, die anstelle von Zahnrädern Aktuatoren mit Kugelgewindetrieb und Seilzug nutzt und damit einen neuen Maßstab in puncto Effizienz und Sicherheit für Cobots setzt.
Mehr erfahrenThomson High-Load Ball Scews Provide Maximum Load Capacity and Longer Life in a Compact Envelope | 2019-02-04 |
KUGELGEWINDETRIEBE | |||
Kugelgewindetriebe - Zoll | — | — | |
Kugelgewindetriebe - metrisch (Nordamerika) | — | — | |
Kugelgewindetriebe - metrisch (Europa) | — | — | |
KUGELGEWINDEMUTTERN | |||
Flansch-Kugelgewindemuttern – Zoll | — | — | |
Flansch-Kugelgewindemuttern – metrisch | — | — | |
Einschraub-Kugelgewindemuttern - Zoll | — | — | |
Einschraub-Kugelgewindemuttern - metrisch | — | — | |
Zylindrische Kugelgewindemuttern – metrisch | — | — | |
WELLENBÖCKE | |||
Kugelgewindetrieb-Wellenböcke - Zoll | — | — | |
Kugelgewindetrieb-Wellenböcke - metrisch | — | — | |
SPINDELN | |||
Präzisionsgerollte Kugelgewindespindeln - Zoll | — | — | |
Präzisionsgerollte Kugelgewindespindeln - metrisch | — | — | |
ZUBEHÖR | |||
Kugelgewindetriebe - Flansche | — | — | |
Kugelgewindetriebe - Abstreifer | — | — |
To provide better service to you on our websites, we and our service providers use cookies to collect your personal data when you browse. For information about our use of cookies and how to decline them or turn them off please read our cookie policy [available here].