Zum Inhalt springen Zur Navigation springen

06/08/2020 | New Thomson Online Selector Tool for Stepper Motor Linear Actuators Simplifies the Purchasing Experience

Kristianstad, Sweden – Thomson Industries, Inc., a leading manufacturer of linear motion control solutions, has launched an online tool that simplifies the selection and purchase of stepper motor linear actuators. The new tool saves significant time by streamlining the selection process for design and system engineers.

Using the intuitive online selector tool, users can quickly and easily find the optimal Thomson motorised lead screw actuator, or rotating screw or nut configuration for their machine design.

“Built upon the successful framework of our existing online product selectors, this new advanced tool allows users to narrow down to their optimal stepper motor linear actuator based on the needs and attributes that they can select within only a few minutes. Our e-commerce capabilities make the selection process even more efficient for users,” said Saurabh Khetan, Product Line Manager - Lead Screws at Thomson.

With this new online selection tool’s visual-based menu, machine designers and builders can find the stepper motor linear actuator that is right for their application with just a couple of clicks. To further narrow their search, users can take advantage of real-time adjustments as defined by filter parameters - all without leaving the page. Additionally, the tool provides an enhanced shopping experience with up-front pricing and lead times, and user-prompted assistance.

The new Thomson online tool for stepper motor linear actuators streamlines the search, selection and overall purchasing experience.

 

The Thomson stepper motor linear actuator selector tool can be found at https://www.thomsonlinear.com/en/products/motorized-lead-screws-products

About Thomson
With more than 70 years of motion control innovation and quality, Thomson Industries is the industry’s premier producer of Linear Ball Bushing® Bearings and Profile Rail Bearings, 60 Case® Linear Shafting, Ball Screws, Lead Screws, Screw Jacks, Linear Actuators, Linear Systems, and related accessories. Thomson invented the Linear Ball Bushing Bearing in 1945 and has set the standard ever since with an unsurpassed set of linear motion control solutions serving global commercial and aerospace and defence markets. Thomson Industries, Inc. has facilities in North America, Europe and Asia with more than 2000 distributor locations around the world.

For more information: Thomson Industries, Inc., 1500 Mittel Boulevard, Wood Dale, IL 60191-1073; 1-540-633-3549; 1-540-633-0294 (fax); Thomson@thomsonlinear.com; www.thomsonlinear.com.

Zum Seitenanfang