Thomson currently has two account systems - one for the website and CAD model downloads, and one for e-commerce. We understand that two logins is an inconvenience and are working to consolidate our systems into one login process. Until we’re able to consolidate the two logins, please follow these guidelines:
When the actuator reaches the end of stroke it needs to stop or risk overloading and damaging itself. There are several ways to protect the actuator from overload when at end-of-stroke which include:
Clutch
Electronic load monitoring
Limit switches
Clutch
Another form of protection can come from simply including a clutch that
will slip when the actuator hits the end of stroke. Simple and
effective. But the system must be designed so that power is not
maintained after the end of stroke is hit or the clutch will quickly
wear out.
Limit switches prevent damage by stopping the motor if the location of the actuator is at a certain point (Limit). There are three basic classifications of limit switches: end of stroke, adjustable or programmable.
End-of-stroke limit switches: Prevent damage to the actuator by cutting off power to the motor to prevent the actuator from moving beyond the maximum and minimum positions.
Adjustable limit switches: Limit switches that can be moved to different locations along the actuator to set limits that are within the maximum stroke of the actuator.
Programmable limit switches: Stroke limits can be set to limit the stroke in operation to a value lower than the full stroke of the actuator. These can be programmed in the control system of the actuator.
To provide better service to you on our websites, we and our service providers use cookies to collect your personal data when you browse. For information about our use of cookies and how to decline them or turn them off please read our cookie policy [available here].