Skip to content Skip to navigation

Installation Instructions


Similar to linear bearings and ball screws, ball splines are are shipped with rust preventative oil (unless otherwise specified). Rust preventative oil is not adequate lubrication for use. Prior to operation ball splines should be lubricated.

The primary objective of the lubricant is to prevent inter-metallic contact of the moving surfaces. Its secondary role is to protect against corrosion and minimize wear. In general, the choice of lubricant for a ball spline or ball screw is similar to a rolling bearing. Small quantities of oil, grease may be used. An important point with shaft lubrication is to ensure that there is lubricant film while the outer race moves along the shaft.

The choice of lubricant often depends on the type of lubrication used in components adjacent to the screw.  However, in general applications - EP2, extreme pressure NLGI grade 2 lubricant is often a good choice.  A lubrication supplier is a good source for recommendations on specific applications.

During the life of the unit it will need to be re-lubricated.  The frequency of lubrication is dependent on:
  • Duty cycle
  • Environment
  • Level of contamination
It is difficult to give a specific recommendation on interval.  Best practice is to ensure that there is lubricant on the spline at all times and adjust the lubrication interval as necessary.
Test your knowledge
back to top