![What is the coefficient of friction for profile rail carriages?](/ds_images/images_relaunch/What_is_the_coefficient_of_friction_for_profile_rail_carriages-585x400.jpg)
The coefficient of friction for ball style carriages is 0.002 to 0.003. Roller style carriages have a coefficient of friction of .001 to .002. In light load applications seal drag, lubrication viscosity, preload, and other factors affect the total actuation force. Please see the engineering section of the catalog or contact application engineering for help calculating the total actuation force.