![What does the clutch do?](/ds_images/images_relaunch/what-does-the-clutch-do_585x400.jpg)
The clutch, commonly called an overload clutch, is a load-limiting device in the actuator that interfaces the gearbox and the screw assembly of the linear actuator (the rod or piston). This, when subjected to a certain load (typically 20-25% higher than the rated dynamic load) will ratchet or slip, preventing the actuator from damaging itself due to overload.