Thomson currently has two account systems - one for the website and CAD model downloads, and one for e-commerce. We understand that two logins is an inconvenience and are working to consolidate our systems into one login process. Until we’re able to consolidate the two logins, please follow these guidelines:
It is set at the end of the production line for each actuator individually. This allows each actuator to be calibrated to its rated load specification, which eliminates problems caused by build tolerances, screw and gearing wear-in, etc.