Thomson currently has two account systems - one for the website and CAD model downloads, and one for e-commerce. We understand that two logins is an inconvenience and are working to consolidate our systems into one login process. Until we’re able to consolidate the two logins, please follow these guidelines:
Can the amperage number or limit be set for an actuator?
Can the amperage number or limit be set for an actuator?
Using the J1939 messages the user can set the number of Amps the actuator is allowed to see before turning off motor current. This feature is similar to a clutch, but different in the fact the user gets to set the load at which the unit will trip.