Thomson currently has two account systems - one for the website and CAD model downloads, and one for e-commerce. We understand that two logins is an inconvenience and are working to consolidate our systems into one login process. Until we’re able to consolidate the two logins, please follow these guidelines:
Can ball screws be used in vertical applications without back driving?
Can ball screws be used in vertical applications without back driving?
Ball screws can be used for vertical applications. To prevent back-driving, a nut anti-rotation mechanism would be required and a back-drive torque applied to the system to maintain the load.