Skip to content Skip to navigation

4/8/2013 | Thomson upgrades linear bearing capabilities in Europe

WOLFSCHLUGEN, GERMANY -  Linear motion specialist Thomson has upgraded its Cut Centre in Wolfschlugen, Germany to provide dedicated local rail customisation and improved service for its linear bearing and guide product lines in Europe.

The investment is in response to increasing demand for its award-winning 400 Series profile rails, that are shipped to Germany in standard 4m lengths for extended joint-free motion. These are then cut to length, matched and assembled to customer’s mechanical and lubrication specifications in Wolfschlugen.

Jonathan Wray, Product Manager Linear Bearings & Guides explained: “Demand had outstripped our local capability to customise products and deliver the high quality components that Thomson is known for. Investing in world-class wet-cutting equipment in Wolfschlugen and developing local hard chrome plating capabilities is the first part of an ongoing programme to ensure high quality, good service and improved delivery in Germany and throughout Europe.”

The new Cut Centre incorporates high tolerance machining capabilities, finishing and etching equipment dedicated to the customisation and assembly of linear bearing rails to customer’s specifications. Part availability has been further addressed with the introduction of new Kanban-controlled inventories for 400 Series and round linear bearings to provide better in-stock availability for customers supplied from the German facility.

Interesting facts about Thomson

With over 60 years of expertise in the field of drive technology, Thomson is the unrivalled industry leader in the manufacturing of Ball Bushing® and profile rail bearings, 60 Case® shafts, precision ground and rolled ball screws, linear actuators, gearheads, clutches, brakes, linear systems and suitable accessories. Thomson launched the linear ball bushing bearing onto the market back in 1945 and since then has been setting new benchmarks in the development of drive control solutions for companies from a wide range of industrial sectors such as the aviation and arms industry. Thomson Industries Inc. has production sites in North America, Europe and Asia in addition to a global network of over 2,000 dealers.

Notes to Editor

High resolution version of the photo available on request.

Thomson, 1500 Mittel Boulevard, Wood Dale, IL 60191-1073; 1-540-633-3549; 1-540-633-0294 (fax); Thomson@thomsonlinear.com; www.thomsonlinear.com.

back to top