Thomson currently has two account systems - one for the website and CAD model downloads, and one for e-commerce. We understand that two logins is an inconvenience and are working to consolidate our systems into one login process. Until we’re able to consolidate the two logins, please follow these guidelines:
Thomson ball screw assemblies consist of a ball screw, a ball nut with recirculating ball bearings and end supports for mounting. The interface between the screw and the nut is made by ball bearings that roll in matching forms in the ball screw and ball nut. The load on the ball screw is distributed over a large number of ball bearings so that each ball is subjected to a relatively low load. Because of the rolling element design, ball screw assemblies have a very low coefficient of friction, which equates to highly efficient mechanics.
Ball screw assemblies provide an excellent method for translating rotational motion to linear motion for many applications, including those where high loads and close tolerances are required. To apply the correct type of ball screw and nut assembly in a particular application, the design engineer must consider the advantages and capabilities of each. Selecting the right technology can reduce design complexity, improve performance and reduce the overall cost of the assembly.
This image compares the three types of ball return systems (from left to right): internal, button and external.
Ball screws are mounted in either supported or fixed configurations. A supported end holds the ball screw at one focal point and does not resist bending moments. A supported end is generally easier to align and install than a fixed one, so installation costs are typically lower. A fixed end resists bending moment loads because it is typically based on two bearings spaced sufficiently so the ball screw remains perpendicular to the planes of the rotary bearings. The fixed offers greater column strength and higher critical speed. The image below illustrates four fixity options.
The assembly can be fixed at both ends, fixed at only one end and supported on the other, supported at both ends, or fixed at one end and free at the other.
Ball screw assemblies are not all alike. Whether it be metric ball screws, inch ball screws or miniature ball screws, key differences affect their performance and extend their lives. These include:
Herhangi bir yeni uygulama, ürün performansı, ömrü ve maliyetinin dikkatli bir şekilde analizini gerektirir. Özellikle daha büyük yükleri üstlenenler. Bir sonraki lineer hareket uygulamanız için neden standart bilyalı vida yerine yüksek yüklü bilyalı vidayı düşünmeniz gerektiğini öğrenin.Sunucu: Markus Brändle, Ürün Hattı Uzmanı - Vidalar, Vidalı Krikolar ve LB&G Thomson Neff Industries, Almanya
Yataklar bir düğme geri dönüşlü bilyalı somuna nasıl yeniden yüklenir. Genellikle Metrik bilyalı somunlar, düğme geri dönüşlü bilyalı somunlardır. Ancak bu teknik, boru dönüşlü bilyalı somunlarda da kullanılabilir.
Binlerce olası seçenek arasından, lineer hareket uygulamanız için en uygun vidalı mil çözümünü nasıl hızlı ve güvenli bir şekilde boyutlandırabilir ve seçebilirsiniz?
Bir milden bir vidaya bir bilyalı somun nasıl takılır.
Bilyalı vidalar hem inç hem de metrik boyutlarda mevcut olduğundan, tasarımcılar bazen ölçü birimine dayalı bir ürün ailesi seçerek spesifikasyon sürecine başlarlar. Bu karar, uygulama için ideal ürünü zamanından önce dışlayabilir ve önemli zaman, işçilik ve masraf kayıplarına yol açabilir. Bu makale, ürün adları yerine performansa odaklanan boyutlandırma ve seçim sorularının nasıl daha verimli lineer hareket tasarımlarına yol açabileceğini açıklamaktadır.
Daha fazla bilgiMakaralı vidalar, boyutun bir kısıtlama olduğu durumlarda büyük yükleri taşımak için tercih edilen tek teknoloji olarak tanıtılmıştır. Ancak gerçekte, bilyalı vida teknolojisindeki gelişmeler artık yüksek yüklü uygulamaları da destekleme özelliğini mümkün kılmıştır. Bu önemlidir, çünkü yüksek yüklü bir bilyalı vida, tipik olarak eşdeğer performans noktalarında karşılaştırılabilir bir makaralı vidanın maliyetinin yarısından daha azdır.
Daha fazla bilgiSürekli kaldırma işlemlerini içeren ancak yine de insan dokunuşu gerektiren büyük ölçekli üretim uygulamalarında kullanılan işbirliği robotları (cobot'lar) popülerlik kazanmaktadır. Bir Fransız cobot üreticisi, dişliler yerine bilyalı vida ve kablo aktüatörleri kullanan ve cobot verimliliği ve güvenliği için yeni bir ölçüt belirleyen bir çözüm geliştirdi.
Daha fazla bilgiThomson High-Load Ball Scews Provide Maximum Load Capacity and Longer Life in a Compact Envelope | 2019-02-04 |
BİLYALI VİDA TERTİBATLARI | |||
Bilyalı Vida Tertibatları - İnç | ![]() |
— | — |
Bilyalı Vida Tertibatları - Metrik (Kuzey Amerika) | ![]() |
— | — |
Bilyalı Vida Tertibatları - Metrik (Avrupa) | ![]() |
— | — |
BİLYALI SOMUNLAR | |||
Flanşlı Bilyalı Somunlar - İnç | ![]() |
— | — |
Flanşlı Bilyalı Somunlar - Metrik | ![]() |
— | — |
Dişli Bilyalı Somunlar - İnç | ![]() |
— | — |
Dişli Bilyalı Somunlar - Metrik | ![]() |
— | — |
Silindirik Bilyalı Somunlar - Metrik | ![]() |
— | — |
UÇ DESTEKLERİ | |||
Bilyalı Vida Uç Destekleri - İnç | ![]() |
— | — |
Bilyalı Vida Uç Destekleri - Metrik | ![]() |
— | — |
VİDALAR | |||
Hassas Yuvarlanmış Bilyalı Vidalar - İnç | ![]() |
— | — |
Hassas Yuvarlanmış Bilyalı Vidalar - Metrik | ![]() |
— | — |
AKSESUARLAR | |||
Bilyalı Vida Flanşları | ![]() |
— | — |
Bilyalı Vida Silecekleri | ![]() |
— | — |
To provide better service to you on our websites, we and our service providers use cookies to collect your personal data when you browse. For information about our use of cookies and how to decline them or turn them off please read our cookie policy [available here].